AXIS#.WARNING#
Description
This keyword can be used to extract individual warnings from the specified axis.
The order of warnings are represented by the order in which the warnings were thrown. For a description of all warnings see Faults and Warning Messages.
Examples
If there were a warning present (4311) is present on Axis 1, it can be extracted by using AXIS1.WARNING1:
-->AXIS1.WARNING1
4311
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read Only |
| Units | N/A |
| Range | N/A |
| Default Value | N/A |
| Data Type | Integer |
| See Also | AXIS#.WARNINGS |
|
Stored in Non Volatile Memory |
No |
Variants Supported
Supported on all device types.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.WARNING1 | 0x5012 | 0x1 | UDINT | - | - | RO | False |
| AXIS1.WARNING2 | 0x5012 | 0x2 | UDINT | - | - | RO | False | |
| AXIS1.WARNING3 | 0x5012 | 0x3 | UDINT | - | - | RO | False | |
| AXIS2.WARNING1 | 0x5112 | 0x1 | UDINT | - | - | RO | False |